AXIS#.MOTOR.BRAKEPOWERLOW

Description

Low voltage used by power saving brake operation (AXIS#.MOTOR.BRAKEPOWERSAVING).


  • This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1 and motor memory version is 0.4 or greater.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Volts

Range

10.602 to 24.002

Default Value

17

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.